Part Number: DS90UB927Q-Q1
Other Parts Discussed in Thread: ALP
Hello,
We can use external video source and feed 927 serializer EVM through to 928 deserializer EVM and on to LCD. Can also generate patterns using serializer or deserializer.
Do still have one funny behavior. With everything hooked up, and with pattern generators disabled in ALP Pattern Generator tab, if driven with external video source and then turn off the external source, I still see a scrolling of patterns. This is not the scrolling pattern I have set up in pattern generator. I see R, G, B, BLK, WHT, checkerboard (looks to be scaled by 16 since squares are good sized), [probably] vertical lines (one pixel wide), and then horizontal lines (one pixel wide).
Have looked through the registers, and don’t see anything that I think would get the EVMs in this mode. It will do this with cable from external video source disconnected (I can power off the drive and disconnect cable while it is in this mode) and it continues this scrolling pattern, so the external source would not seem to be the problem, and I can disconnect cable from serializer to deserializer and it stops, so probably not the deserializer.
Might there be some register setting in the serializer that I have inadvertently left set that puts it in this mode?
In serializer register 0x03 I can disable PCLK_AUTO to kill this behavior, but why is it scrolling?
Thank you,
Ryan B.