Dear Sir,
What are the requirements for camera synchronization of ds90ub964? how large is the internal buffer, and the margin out of sync can it be?
if there is a camera project, We need three cameras to look back, one camera to do face recognition, and the rate of each camera is different. The three cameras of back view are all 720p, and the resolution of face recognition camera is 1280*960.
Would you please confirm whether the DS90ub964 can meets this asynchronous feature requirement?
If not, whether the TI has a suitable chip to support this application,thanks a lot.