Part Number: DP83848C
Hello there!
I have made a custom board with Eagle (Autodesk), I used the PIC32MZ2048EFH64 with a dp8384 Ethernet physical layer transceiver. Also a few other things, like regulated voltage supply and i/o ports (the basic stuff).
I can program the pic etc, working fine. But I do have problems with the dp83848, and it maybe looks like a hardware problem?the strange thing is that when I put a ethernet cable at my rj45 and so I connect it to my phy,
The strange thing is that the lights doesn’t blinks on, On the rj45. Without Any software it should detect a connection with the network or switch right?
I also tried a cross over cable, I thought maybe it had to do something with that.
Because my board has a tap ub rj45 connector, so it is the same as a switch TP-Link right, so I need a cross over.
But that didn't fixed the problem ass well for the led Activity situation.
I will put down a schematic of the situation, I think the part of the PIC microcontroller doesn't matter a lot for the problem now. Because I cannot ping the device, but the problem already starts in my opinion by not see the activity and LINK led ON, ass wel on the rj45 connector as the switch.

Hopefully there is someone out there that can help me!
Best regards,
Marc