Part Number: TLK10031
Other Parts Discussed in Thread: TLK10022, TLK10081
Hello,
In my application,the XAUI interface of PPC is connected with the low-speed side of TLK10031, SFP+ is connected with the high-speed side, and the 10,000-mega network card is connected with the optical fiber cable. The link lamp of the network card is not on.Using optical fibers connect two same TLK10031 boards, the AN_STATUS registers are accessed through MDIO interface. Bit 2 (LINK_STATUS) is unstable, and 0 and 1 are always changing.
What should I pay attention to? How about the correct configuration?
Please reply as soon as possible.