This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65LV1224B: LVDS Deserializer

Part Number: SN65LV1224B

Hi,

We are using the  SN65LV1224B in our design; however, the datasheet does NOT provide enough information to enable us to create the schematic symbol. We are using the Quad Flat Pack package, and we don't know how to determine what are the pin numbers are for ROUT0, ROUT1,.....ROUT9. Please provide us with this data.

This is the datasheet that we are using:

www.ti.com/.../sn65lv1224b

Thank you,

Glen

  • Hello Glen,

    Sorry that the pinout is not clearly indicated in the datasheet for the deserializer. We are working on fixing that in the next rev of the datasheet. The pin assignment are in the Pin Functions table on page 6. Rout0-Rout9 are pins 27-23, 18-14. So, Rout0 is pin 27, ..., Rout4 is pin 23, Rout5 is pin 18, ..., Rout9 is pin 14.

    Regards,
    Yaser