Part Number: TUSB8044
Hi Team,
My customer would like to know about clock input.
Regarding the clock input, is there a specification of the minimum value maximum value of VH and VL?
The clock oscillator that my customers want to use is as follows.
Can they use it?
VH min 90%VDD = 1.62V
VL max 10%VDD = 0.18V
Also, is it necessary to pull down D + D -?
(In TUSB 2036, it was necessary to pull down with 15 KΩ for detection to D + D -)
Best Regards,
Kenji