Part Number: LMH1983
Hi Team,
Please advise me two questions bellow.
The LMH1983 datasheet “8.3.11.1 TOF3 Initialization Set Up” insists that it is
recommend setting PLL3 into “Always Align mode” to firmly Reset PLL3.
Q1. When the PLL3 is reset?
Does the PLL3 reset at top of frame 1 (TOF1) or top of frame 3 (TOF3)?
Q2. When 10 MHz, 27 MHz, 96kHz, 48kHz, 44.1kHz 32 kHz or unknown video is
Applied to the REF input, how much the period of FOUT1?
Mita