This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS16EV5110: How to detect the normal problem of output image with DS16EV5110

Part Number: DS16EV5110

Dear sir:

I have a question. Please give me an answer. How to detect the normal problem of output image with DS16EV5110。Is there a register to monitor?   

  • Hi David,

    The only indications are signal detect pin (Pin# 45) and reg 0x01 and 0x02 which indicate enable pin and boost settings.

    Normally, DS16EV5110 is used on the sink side. I am thinking it would be a good idea to have FPGA check incoming signal and then change EQ boost settings to optimize incoming signal eye opening.

    Regards,,nasser