Part Number: DS10BR150
What will happen if the part is used with the inputs not connected. In our application a cable will be used to connect an LVDS driver to this buffer but I just want to make sure the part does not start oscillating when the inputs are disconnected from the cable? Is there a default output value? Or should we slightly bias the inputs to ensure a default value... We have a modest datarate of around 200Mbps.