This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CApacitive Load driver



I don't know if this is the correct forum, but I am interested in generating a 48Vac waveform to drive a 1uf capacitive load. Is there any driver that could support this?

Thanks

  • Hi Tom,

    Thanks for using E2E, and to help get an answer for you, please provide some additional details.   Such as:

    Frequency of the signal? 

    Fixed freq or adjustable? 

    Amplitude of the signal 48VAC RMS or p-p? 

    Sine or Square wave (or another shape)? 

    Any resistive or inductive load in parallel with the 1uF cap? 

    Do you plan to generate the wave using a uC to DAC, or some other method? 

    A block diagram of your concept would also be helpful. 

    Regards,

    ~Leonard  

     

     

     

  • Thank you Leonarad,
    I am looking for a variable 48VACpp 60Hz squarewave.
    I want to drive the wave with a little micro too.
    Thank you.
    Regards,
    Tom