Part Number: TPS65987D
Hi Team,
My customer considers to design their application with TPS65987D.
The requirement of the application is the following.
- Source power (up to 60W) to note PC that is connected to Type-C receptacle of the application with USB 3.1 & 2.0 communication.
I believe Power Role Swap is required in this application and I would like to ask the following.
---------------------------------------------------------
1) Is it possible for TPS65987D to do the power role swap in stand-alone (no external controller)?
2) Can TPS65987-90EVM be used to evaluate the power role swap function?
---------------------------------------------------------
Best Regards,
Yaita