Part Number: DS90LV018A
Other Parts Discussed in Thread: DS90LV017A, DS90LV012A, DS90LV011A
Hello everyone,
I'm interested in the DS90LV018A and the DS90LV017A to convert TTL 3.3V signal to LVDS 1.8V signals (and vice versa).
Are these two components allowing that ? If yes :
- For the 017A (driver) :
==> How can I know the output of my driver is LVDS 1.8V if I power the component with 3.3V (Vcc) and have an input of 3.3V TLL.
==> Do I have to add a resistor somewhere ? (for impedance)
- For the 018A (receiver) :
==> Do I have to power the Vcc with 3.3V so that the TTL output is TTL3.3v ?
==> Do I have to add a resistor at the entrance of my receiver (100 ohm in the datasheet) ?
Thanks a lot for your answers (it's kind of blurred for me right now).