Hi team,
The customer is considering building some prototypes of the LV-TTL RGB to HDMI bridge board with TFP410.
(1) Is I2C setting needed for the TFP410 operation? Can the customer use this device without I2C configuration?
(2) Can this device output HDMI data (without audio) only by the input of RGB-24bit data and clock?
(3) What is the recommended ESD protection device for the input side(RGB) and the output side(HDMI), respectively?
(4) What is the recommended translator device between the LV-TTL RGB data and the input of TFP410?
(5) Can you provide the reference schematic for that use-case (LV-TTL RGB 24bit to HDMI, 1920x1080/60p)?
Thanks and Regards,
Ishida