Part Number: SN65DSI85
Other Parts Discussed in Thread: DSI-TUNER
I have a test pattern running, it seems to be going fine for a few minutes, but then the output abruptly stops. All the registers are still set. Any idea what could cause this?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1. Is the LVDS CLK still running when the output stops?
Yes 74.25Mhz, it comes from a 1.8V powered oscillator.
2. Are you configuring all the registers before setting the PLL_EN bit?
I wasn't but I moved it to the end of my configuration script, and same result
3. Are any bits being set in error register 0xE5/0xE6? (Please clear these registers by writing 0xFF to them before reading them)
Yes I cleared them with 0xFF at the start of my script 0xE6 was 0x40 0xE5 was 0x01, but it's always 0x01 even in our other production 720p systems that use the DSI83.
Clearing these bits again, and trying a soft reset doesn't bring back the test pattern.
4. Is the external reference clock within the electrical and switching characteristics of the datasheet?
I believe so, it is 74.25Mhz at 1.8V. It is the same oscillator we use in our production DSI83 based systems.
5. Are you able to try generating the test pattern by using the DSI CLK instead of an external reference clock (ensure to follow the initialization sequence in the datasheet)?
No, that is supposed to happen after we prove that the DSI85 is working with the test pattern.
6. Can you share your display datasheet and register settings. Sharing the settings with the DSI-Tuner would be preferable, and you can email the display datasheet to i-anyiam@ti.com if you do not want to share it on this forum.
I don't think so, it's under NDA and TI could be considered a competitor with your DLP displays.
I can share the timing:
| lines | hex | clocks | hex | |||
| lines | 1080 | 438 | active pixels | 1920 | 780 | |
| vsync | 5 | 5 | hsync | 44 | 2C | |
| vertical back porch | 36 | 24 | back porch | 148 | 94 | |
| vertical front porch | 4 | 4 | front porch | 88 | 58 | |
| total | 1125 | 465 | 2200 | 898 |
pixel clock is 148.5MHz
%CHIP3%PVCAraon-tech%PMCARDC200%RPCA1920%RLCA1080%PVCB%PMCB%RPCB%RLCB%LVCM0%HPWA44%HBPA148%HFPA88%HACA1920%HTOA2200%HPWB%HBPB%HFPB%HACB%HTOB0%VPWA5%VBPA36%VFPA4%VACA1080%VTOA1125%VPWB%VBPB%VFPB%VACB%VTOB0%PCKN148.5%LCKS1%RCKM74.25%MULT1%DCKA%DIVI0%LCKR148.5%FMTA1%DEPA0%HSPA1%VSPA1%BPPA1%FMTB1%DEPB0%HSPB1%VSPB1%BPPB0%PRDA1920x1080%PRDBx%DSCM0%LREO1%LRCE1%LPCA0%BMCA0%SMCA0%LPCB0%BMCB0%SMCB0%DHPA44%DHBA148%DHFA88%DHAA1920%DHTA2200%DHPB%DHBB%DHFB%DHAB%DHTB%DVPA5%DVBA36%DVFA4%DVAA1080%DVTA1125%DVPB%DVBB%DVFB%DVAB%DVTB%DDRA1039.5%NOLA3%VIMA0%LCRP%DDRB%NOLB0%VIMB0%RCRP
Here's the output from dsi tuner, I had to add the .txt extension for the website to allow me to upload it.
Here's the output from dsi tuner