Part Number: TPS65987D
Hi, everyone,
We designs PC & tablet using TPS65987DDH.
Now, we have trouble with PC when attaching PD monitor.
Sometimes PD monitor is still dimmed.
And we've noticed something wrong with PDC.
- HPD won't become HI, when PD monitor is attached,
even if PD negotiation is finnished properly. (We've checked "EnterMode" is issued)
- High voltage Warning (0x29 register) becomes HI, only when we remove PD device.
(Sometimes, both of High / Low Voltage Warnings become HI.)
And also, we know HPD becomes HI and Voltage Warnings are cleared,
if we reset PD controller by HRESET pin or software reset command (4CC).
[Question]
(1) Why HPD won't become HI even if PD monitor is attached?
(2) Are there any tips to clear High / LowVoltageWarning?
Status (0x29) register is for read only, so we cannnot change these bits by EC.
(3) Are there any countermeasures against this problem?
And are there any relation between HPD failure & High/LowVoltageWarning?
(4) We are planning to use "4CC" command as the countermeasure (SW reset).
For examle, "GAID".
Could you tell us what "4CC" command is best?
Because we're worried about side-effect of "4CC" commands.
Best Regards,