Part Number: TUSB2077A
Other Parts Discussed in Thread: TUSB2036
Tool/software: Linux
Hi,
I have customized boards on which TUSB2077A HUB IC is connected to USB pins of a SOC. The SOC supports for both Andrioid and Linux OS.
The reset circuitry for the active low RESET pin of the TUSB2077A IC as mentioned on page 11 of "TUSB2036 and TUSB2077A EVM User's Guide" (sllu190.pdf ) is as follows.
For both the OS sometimes the USB hub seems to be working perfectly but sometimes the USB connectivity just randomly goes off. On some boards re-flashing the OS brings back the connectivity where as on some the connectivity is still down.
But when I replace the capacitor of 0.1uF with 1uF the USB connectivity is regained.
Can anyone please explain me what exactly is the issue occurring over here? and is there any solution from software side for this issue?