We have a SN65DSI83 on our PCB, and are attempting to communicate via I2C.
The address pin is pulled high (to 1.8V) and the enable pin is also tied high (to 1.8V). But we get no response from the IC.
We have plugged into the development board, and can communicate withe the SN65DSI83 on that, so we must be doing something wrong with the wiring of the SN65DIS83 on out PCB.
The REFCLK line is pulled to 0V via a 10k resistor, the I2C lines are pulled up via 4k7 resistors. The 1.8V and the 1.1V rails are both up and stable. Yet the SN65DIS83 is still not responding.
I tried this on one PCB, and pulled the enable pin to 3.3V, so suspect we've damaged the SN65DIS83 on that board. But have tried it on a couple of others, which have the enabled pin pulled to 1.8V.