Hi!
I need serial subLVDS to parallel CMOS interface converter for imx290 in 1080p30 mode.
I have not found a suitable deserializer and I want to use sn64lvds324.
It is necessary to convert 4 serial 111MHz subLVDS channels into one parallel 12 bits 75MHz.
Is it possible to use the sn64lvds324 in the deserializer mode :
input 1 port 4 channel 111 MHz
output 12 bit 75 MHz
without using Vsync/Hsync signals?
I just need a word recovery mechanism..
Best regards.