Part Number: AM26LV32
Hello,
I'm looking for a Quad RS-485 receiver with low tHL/tLH<~20ns.
I found the AM26LV32I. There is a conflict between the parameters mentioned in different places in the site.
1. Is this component available? (with the "I" at the end).
1. Is this component fully compatible for RS-485 communication standard, and what is the termination required in multi drop usage (from one transmitter to X receivers)?
2. What is the allowed number of receivers to be connected on a single lane? (one place says 32, other 10, not mentioned in the datasheet).
3. Is the SN65LBC173A preferred? (although it seems to be older, and it has SOIC package only).
Thanks!