Part Number: DS90UB953-Q1
Other Parts Discussed in Thread: ALP
Dear Sir,
Is there any method to trigger two ds90ub953 internal pattern at the same time? two ds90ub953 are forwarding to ds90ub954 by line concat mode, in ALP information tab, Current CSI TX status show:
Pass Sts: No or yes this bit showes No or Yes ,while running
Sync Sts: No, this bit showes No always, while running
So How to trigger these two ds90ub953 to generate sync streams in the same time?
Thanks