Part Number: TUSB4041I
Hi,
customer use TUSB4041I, has below quesitons, could you give some comments?
1. in the datasheet, below table 7.6, the (2) say the VDD must be stable minimum of 10us before VDD33, but the figure 1 show the VDD33 should be stable before VDD. I'm confuse about it. which one is normal power -up timing? Meanwhile, the page 14, 8.3.7 say, the device does not specific power sequencing requirements. I wonder if there any mistaks?
2. what's the meaning of tsu-io and thd_io?
3. customer place 1uF in GRST pin, VDD and VDD33 power up at the same time, one board can work and other one not. Why?
4.They use external circuit to control GRST voltage, GRST=0 before VDD and VDD33 stable, and then wait 3ms, pull GRST to high. in this condition, circuit can work properly. is there any potential risks?
thanks for your attention.