Part Number: TCA9509
Other Parts Discussed in Thread: TCA9803
I specifically need a part that has a high impedance on SDA and SCL when the power is removed from Vcca and Vccb. The "Features" section of the datasheet (SCPS225C - August 2011) indicates "Powered-Off High-Impedance I2C Bus Pins." However, I cannot find a specification in the data sheet that indicates parametrically that high impedance on SDA and SCL will occur when the power is removed.
My application is an SMBus where the master processor on board will be powered off (on the Vcca power rail) and a programming tool will power up the circuit subsection for SMBus (Vccb side) but I do not wish to power Vccb on this device.
My rationale for not powering Vccb while programming is that I have limited power available when the SMBus is operating (Vccb) and if I power Vccb from the power rail that my programming device uses, under normal operating conditions I may draw too much power from the isolated power rail that I have available for Vccb.
I believe that the part will meet my needs but I want to be sure before I spin a very expensive FPGA board with this part on it. If I cannot program the SMBus enabled power supply manager with my programming tool when the power is removed from Vcca and Vccb, I will not be able to power up my board without removing this voltage translation device.
If there is another part that parametrically specifies the condition that I'm considering, please inform me. My needs are simple: 400Khz max Vcca = 1.8V, Vccb=3.3V, and SDA and SCL on the Vccb side must be high impedance when power is removed from Vcca and Vccb.
Regards,
Paul Eason