Part Number: TCAN4550-Q1
Other Parts Discussed in Thread: TCAN4550
Datasheet 8.3.3 Vccout PIn says,
When a bus fault happens and requires the maximum of 100 mA from the regulator the device will not be able to source 70 mA to external components.
My understanding is that when a bus fault happens and if the required current is less than 100mA, Vccout will still be available, am I correct?
Customer hopes the Vccout will be always available even if fault happens. Thanks.