Part Number: DP83848C
Hi.
I have a problem with the title and want to find the cause and solution.
Refer to the data sheet [Figure 7-1. Typical Application Schematic] & [Figure 7-2. 10/100 Mb/s Twisted Pair Interface],
Pulse magnet (hx1260nl) was used and the circuit was designed.
problem is :
It is possible to connect 1: 1 connection with PC and Ethernet routers,
but when connected through Ethernet switch (Advantech EKI-2525I), only link LED operates and does not perform any operation.
Unfortunately, the JTAG interface is not configured.
Can you infer the cause of this problem?
Thank you reply
Hosung HAN.