This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS125MB203: Mode pin connection

Part Number: DS125MB203

Hi team,

For the mode pin, there is 4 level and we recommend to connect the pin using the pull up or pull down resister.

My customer only need level 0 and level 1, can they use the FPGA GPIO to direct control the pin and don't connect the pull up or pull low resistors?

For example, in order to control the SEL0 to level 1, the GPIO of the FPGA output a high level voltage direct to the pin SEL0, will this cause issue?

Lacey

Thanks a lot!