Part Number: DS90UB954-Q1
Hello,
Could you please suggest the registers configuration of 954 when it's paired with 933?
Input format of 933 is YUV422, using lower 8-bit, resolution 1280*720. 954 use RX port 0, with 4 MIPI lanes/400M.
Below is the configuration customer used but they failed to get the output data.
0x0C 0x81
0x20 0x20
0x21 0x01
0x33 0x41
0x4C 0x01
0x58 0x58
0x6D 0x7F
0x7C 0xE3
0xBC 0x1F