Part Number: DS90UB962-Q1
Hi, I want to use the BIST mode in ub962,and have some doubt:
1. to enable the BIST, only need to set reg 0xB3 to 1?
2. how long will the test last? or only stop when set 0xB3 to zero?
3.how to view the test result? to read reg 0x57? there are four cameras connect to ub962 , why there is only one reg to read?
4. if the reg 0x57 is 0 , do it indicate the test pass? and if not zero, do it indicate the test fail?