Other Parts Discussed in Thread: DP83869, DP83867CS
I need to go from RGMII to optical 100Mb then on the other side to copper Etrhernet. This is a closed system, I can use any protocol and configure the chips any way needed.
The DP83869 looks like a good choice for this. I see two different ways to set this up:
Strap to RGMII > 100BASE-FX > fiber > 100BASE-FX > copper Etehrenet. The RGMII side looks like it can be done with just strapping. The closest strapping on the other side seems to be SGMII > Copper Ethernet. Can the SGMII be configured to 100BASE-FX?
Strap the RGMII side to RGMII > SGMII and turn off auto-negotiation and set speed to 100, then the next DP83869 strapped to SGMII > copper Ethernet and again turn off auto-negotiation, set speed to 100 ans setup MDI auto-negotiation to 100 only.
I would prefer the first one since I only need to program one of the DP83869s, but programming both is certainly fine if I have to.
Other quick question, when will distributors start carrying the part?
Thanks,
John S.