Part Number: TPS65983B
Other Parts Discussed in Thread: TPS65982
Hi there,
At present, the customer has a project evaluation. The Thunderbolt design uses two external PD chips from Alpine Ridge DP. The two PD chips are connected to one Thunderbolt output. Currently, it is estimated to use TPS65983B (support PD3.0). Currently have the following questions to ask:
1. Can the TPS65983B meet the requirements of TBT certification when it is designed with Alpine Ridge DP for one to two (one alpine ridge out of two TBT ports)?
2. When designing the PD, I have a question here. The PD chip BUSPOWERZ is used to configure VBUS to the system channel (decharge) in the case of dead battery or NON-battery. Please ask this configuration on the VIN_3V3 of the PD chip. Is there still work in the case of electricity?
BR, Eason