This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB933-Q1: If DS90UB933-Q1 supports 2M images, how should it be designed?

Part Number: DS90UB933-Q1

If DS90UB933 is used to transmit 2M images:

1. There are only 12 input interfaces of DS90UB933, and the image interface can only be accessed according to yuv422-8bit.(specify YUV422)

2. Effective pixel points of 2M image: 1920*1080*30*16/8 = 118.65mbyte, that is, at least 120MHz of PCLK output.

3. The input PCLK of DS90UB933 supports a maximum of 100MHz.

If DS90UB933 supports 2M images, how should it be designed?