Part Number: PCA9306
How large current can VCC and VCORE consume?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
There is no pin namd "VCORE".
Assume that current flows through the 200 kΩ resistor to the lowest input voltage; with 5 V to ground, this would be 25 μA. And there is the input leakage current (less than 5 μA).
Otherwise, there is no power consumption in the PCA3906. For practical purposes, the power consumption is entirely determined by the currents through the pull-up resistors (which also flow through the switches).