This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65DPHY440SS: Implement position and signal distance

Part Number: SN65DPHY440SS

Hi team,

Several questions for SN65DPHY440SS

1. Can SN65DPHY440SS be placed on the camera side or the SOC side instead of the middle position between camera and SOC?

2. How long can the signal be transmitted after SN65DPHY440SS? can it support 50cm?

3. If SN65DPHY440SS can't be placed on the camera side or SOC side, what else can you recommend to support MIPI CSI to transmit for 50cm length? Like a pre-emphasis to make it transmit longer or an EQ on the SOC side can recover after 50cm length transmission.

Thank you.

Best Regards

Jack Chen