Part Number: DS90UA102-Q1
Other Parts Discussed in Thread: DS90UA101-Q1
Hi all
Would you mind if we ask DS90UA102-Q1.
The customer uses following devices;
SER : DS90UA101-Q1
DES : DS90UA102-Q1
Register setting : Default
Power source : LDO within specified noise level
And then, they have Lock status.
However, SCK clock at the DES(DS90UA102-Q1) is half of SER's clock.
-SER's SCK clock : 12.28MHz
-DES's SCK clock : 6.14MHz
It seems that SCK signal and Dout signal syncronize.
So, we assume that there is some problem at DES side.
We would like to break down the issue into parts.
Now, we don't have good idea, so if you have the same experience and good advice, could you share us?
Kind regards,
Hirotaka Matsumoto