Part Number: TCA9555
Hi Team,
Customer wants to know if this device has internal latency spec? The time measures from I2C command received to actual output state change.
A typical number should be also fine.
Thanks!
Andrew
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCA9555
Hi Team,
Customer wants to know if this device has internal latency spec? The time measures from I2C command received to actual output state change.
A typical number should be also fine.
Thanks!
Andrew
Hey Andrew,
Section 7.7 of the datasheet mentions a parameter abbreviated as tpv which states the maximum time from the 70% value of the 9th clock cycle of a write to when the port changes is dependent on Vcc. For Vcc between 2.3V to 5.5V the delay is about 200ns.(Note this is for a 100pF load on the output port).
Essentially this means that you should see the ports output before the I2C line even sees a stop condition.
Thanks,
-Bobby