Part Number: SN65LVCP114
1、what is the I2C_SEL pin internal circuit structure? when use GPIO mode ,if can be floating ?
2、When use GPIO mode ,how to deal with the I2C_SCL/I2C_SDA ,if can be floating?
Thank you !
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN65LVCP114
1、what is the I2C_SEL pin internal circuit structure? when use GPIO mode ,if can be floating ?
2、When use GPIO mode ,how to deal with the I2C_SCL/I2C_SDA ,if can be floating?
Thank you !
Hello!
The datasheet discribes the pin with pullup and pulldown for HIZ,if I can make the pin float for HIZ when use in the following circumstance?
I2C_SEL has an internal 48K pull-down. This pin does not require any external components to use GPIO mode.
When in GPIO mode the SCL and SDA pins do not require any external connection, I would still recommend to have a 10K resistor pull-up (DNP) on both pins. This way the device could be exercised in I2C mode by populating the resistors on the board layout