Part Number: DS90UB913A-CXEVM
Other Parts Discussed in Thread: DS90UB953-Q1EVM, , DS90UB913A-Q1
Hi,
We design a tester to test board with 8 ports CAMs using 8 [DS90UB953-Q1EVM]. And we were able to test 6 of the ports. Then we informed that the other two ports need different format and they accept TI913 Serializer format.
Q1) Can we use the DS90UB913A-CXEVM Serializer to generate image patterns similar to the TI953? Any information about setting the pattern generator registers/ Hardware setup?
Q2) is there any spatial pattern image format can be generated using TI913 and cannot be generated by TI953?
The information I have about the required image:
• Simulate 1M camera:
• BT.601 or BT.656, DVP protocol (8 bit)
• Upper 8 bits are used, External H-Sync and V-Sync signal lines
• YUV422 (YCbCr)
Thank you,
Aziz,