Part Number: TUSB1211
Team,
My customer is questioning the internal PLL jitter performance, which is not listed in the spec.
If they supply REFCLK in with 19.2MHz clock, and the clock phase noise is
-90dBc@10Hz, -100dBc@100Hz, -110dBc@1kHz,-125dBc@1MHz,-135dBc@5MHz. And they are asking about the 60MHz output clock's jitter. Could we provide?
Best Regards,
Peter Wei