Part Number: DP83867IR
Our application is highly customized with extreme size constraints and requires discrete magnetics, so we’re forced to place the DP83867IRRGZT on the backside of our pcb directly opposite the magnetics (Pulse Eng Part No: HX5120NL). Our PCB has 20 layers so we’re thinking of routing chassis ground under the magnetics on layer 2, and routing circuit ground under the DP83867IRRGZT on layer 19. The intent is to use chassis ground and circuit ground to shield the DP83867IRRGZT/traces from the magnetics, while still getting ~50mils of separation (distance from layer 2 to 19) between chassis ground and circuit ground. Can you please let us know if this is viable, or if not what the issues with this approach are? BTW, we did see the note in Fig. 40, pg 118 of the datasheet calling for power/ground planes to be voided under the transformer but we’re very concerned that if the planes are voided, in our case fields from the transformer will couple into the DP83867/traces opposite the transformer because the transformer and DP83867 are directly opposite each other on top and bottom of the pcb.
Thanks -John