Part Number: TUSB1210
Other Parts Discussed in Thread: SN74AVC16T245, SN74AVC4T245, SN74AVC8T245
I need to interface a voltage level translator between my TUSB1210 ULPI pins (@1.8V) and a Lattice ECP3 Versa development board that only has a 3.3V voltage option. I have no way of changing development board rail voltage.
I would like to use an Auto Direction Sensing voltage translator for the data pins (I/O), i.e., TI LSF0108QPWRQ1, but this can only auto sense for outputs that are open drain. Therefore, I need to know if the TUSB1210 data pins are open drain or push-pull. The ULPI CLK pin (60 MHz) and other ULPI pins, are uni-directional so auto direction sensing not required.
There are also other auto sensing translators to choose that will only do push-pull or open drain.
Thank you, Roland