This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65988: TPS65988 Slew rate control and SRPOS.

Part Number: TPS65988

Hi Experts, 

The Power switch spec of TPS65988 shows the parameter below.

Does TPS65988 control the slew rate of SRPOS ?

  • Hi Alan,

    The TPS65988 will control the SLEW Rate when transitioning from 0V to 5V on VBUS. However, if there is another transition from 5V to a higher voltage, the TPS65988 will not control the Slew Rate. In those cases, the TPS65988 relies on the DC/DC converter to control the slew rate of the voltage change.

    If this answers your question, PLEASE select This resolved my issue

    Thank you,
    Eric