This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ALP: Scripting GPIO and PWM signals from 929/928 ALP

Part Number: ALP


Is ALP capable of generating a PWM signal from GPIO on 928 deserializer via scripting or an alternative method? Additionally, can the GPIO easily be sequenced if, for example, it needed to sequence other IC's enables on start-up?

Are there any script examples available doing this? 

Regards, 

Logan

  • Logan,

    Yes, you should be able to use scripting to generate PWM signal from GPIO on 928. Please refer to UB928 Data Sheet page 27 for GPIO enable and configuration. If using UB925, please use GPIO3/GPIO2 to transmit control signal.

    I can look and let you know if I find an example script.

    Thanks,
    Vishy