This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi e2e
I used the DS250DF410EVM as a PRBS Checker,how does it worked of DS250DF410 can checked the signal in is PRBS7,PRBS15 or PRBS31.
there has no no reference clock in for channel 2 or channel 3,but it can lock to the signal in and worked as a PRBS Checker?
thank you.
Greetings,
1). DS250DF410 can automatically check incoming PRBS pattern and indicates if it is PRBS7. PRBS31, and etc.
2). Externally - through 100-ohm input of the 2nd channel- we should connect a differential cable or trace to the input of the PRBS checker channel.
Please below note an E2E case discussing this in more details.
https://e2e.ti.com/support/interface/f/138/p/701759/2586513#2586513
Regards,,nasser