Part Number: TUSB564
Other Parts Discussed in Thread: TUSB1064
Hi teams
My customer is using TUSB564 for new design as DP sink device re-driver.
They use a MacbookPro as DP source and connect with DP sink device with a 1.5 meter long cable.
They found the display picture unstable in the DP sink device.
Below is the question:
- Lowest input DP differential voltage level(peak to peak) in TUSB564 input side to ensure robust DP signal transfer?
- Do you have any guideline about how to tuning the EQ parameter to achieve the best robustness?
- In datasheet application circuit(Figure.27) there is no AC-coupling capacitor between RX1/RX2 pairs, i wondering why?
- There is no impedance matching guidance for DP and USB port, but I found the guidance for TUSB1064. In this document it indicates that the length between Type-c connector and TUSB1064 should less than 2 inch with 90 ohm differential resistance. And USB port to device should less than 6 inch and DP to device should less than 8 inch. Are the requirement is the same to TUSB564?
- The timing requirement spec for the signal after re-driver? (How to confirm the signal after our re-driver is meet DP1.4 standard if we don't have the mask for the eye diagram?
Thanks in advance.