This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Network Interface Card ( NIC ) with PCIe



We are planning to develop NIC with PCie interface to the PC  & 1Gbps SFP ( Fiber Optic ). The application is to build single direction NIC card with VCSEL laser diode ( either Tx or Rx ).

1) Suggest us a Ethernet Controller with PCie & SerDes Interface with MAC.
2) Also suggest us, if you have any VCSEL & PIN Laser Diode related driver IC's from NXP.
3)Or You can suggest us a MCU or a processor with both PCie & SerDes capability.
4)Or if any other suggestion.

  • Hi Sharvy,

    A number of companies produce PCIe to Ethernet controllers. We do not have one in our portfolio.

    The way our E2E forum is designed, this question is routed to the Ethernet team because your post's title has to do with Ethernet. If you wish to ask a question in addition about VCSEL & PIN Laser Diode related driver ICs, you will need to make another post in the Data Converter forum.

    For a MCU or processor recommendation, post a new question in the Processor forum.

    Best Regards,