Part Number: DP83869HM
Tool/software: WEBENCH® Design Tools
Dear sir:
I have a few questions to ask.
1.Can this chip support optical input, RJ45 output, RJ45 input and optical output in MediaConvertor mode?
2.Media Convertor mode has two kinds of 1000M and 100M. Can these two modes switch automatically? Or if the chip can detect the change of input signal, MCU can set these two modes by reading the change of state.
3.Is the three PINs of LED_0~LED_2 not the output of the state lamp? Do they need to be connected with the default pull-up or pull-down?
4.Media Convertor can be set by configuring OPMODE_0~OPMDOE_2 at high and low levels, or must it be set by software.