Part Number: DS90UB953-Q1
Hello.
Can the DS90UB953 support the sensor as follows? Or there are other serializer products that can be supported. Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB953-Q1
Hello.
Can the DS90UB953 support the sensor as follows? Or there are other serializer products that can be supported. Thank you.
Hi,
Pls check whether the video color space is RGB888, if yes ub953 can't support it. You can get the csi2 bandwidth of ub953 in the d/s.
For other products to support 3M or higher, pls contact it with TI local team. Thanks.
regards
Steven
Hi, what is your RCCB?
for UB953, it is compliant with D-PHY v1.2 and CSI-2 v1.3 Compliant System, all the data types are defined in CSI2 V1.3.
if you concern the data rate, you can calculate the total CSI2 bandwidth, or you can check the imager (ISP or sensor) output CSI2 rate (should not be greater than 832Mbps per lane at 4lanes setting).
regards,
Steven