Part Number: MAX3243E
Other Parts Discussed in Thread: MAX3243
HI
When my whole device is no powered , and MAX3243 all pin (include DIN, FORCEOFF, FORCEON) are floating,
but there is a 10V(or there voltage) on RS-232 Input/ output pin,
is possible cause vcc or any pin become abnormal ???
, like 3V on VCC , some pins become on certain voltage level.