Part Number: DS90UH948-Q1
Hello,
I understand UH948-Q1 uses internal test pattern generation based on AN-2198 as shown in the datasheet on page 104. The AN-2198 shows table 2 and it says below the table that "internal oscillator reference frequency variation of 140MHz(min), 200MHz(typ) and 260MHz(max) respectively". It should include the variation of PVT(Process, Voltage, Temperature). However my customer sees 139MHz even at room temperature. Is it normal? Or is the unit bad one? Does it really include PVT? Would you please tell me the actual min/typ/max?
Best Regards,
Kawasaki