This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83867IR: Magneticless/AC capacitor operation.

Part Number: DP83867IR

Is it possible to use the DP83867IR "Magneticless" i.e. ac coupled with capacitors?

If yes, are there any constraints: Max Length?, fixed data rate?, no auto-negotiate? etc...

Our length is less than 1 Meter, & we could fix our rate at 100Mbps if need be.

We're working with a processor that lists only 10/100/1000 Ethernet Phy's as supported and there's a lot of legacy with the DP83867 with our processor, so we're reluctant to design it out.