This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB948-Q1: DS90UB947 and DS90UB948 GPIO Remote level

Part Number: DS90UB948-Q1

Serializer DS90UB947 VDDIO connect 1.8 V level, DeSerializer DS90UB948 VDDIO connect 3.3 V level , GPIO control from remote Serializer,   DeSerializer DS90UB948  GPIO level  is  1.8V ;

why  948 GPIO output level consistent with 947 VDDIO , not consistent with the 948 VDDIO ?

Note :  To achieve the function of  " GPIO control from remote Serializer, output level consistent with 948 VDDIO "